Search term

Schaeffler demonstrates pioneering spirit and innovation, and is instrumental in shaping the fully-electric future of the DTM

Pressrelease Stage Image
The demonstration car generates just short of 1,200 hp with 880 kW.

2020-11-06 | Herzogenaurach

  • Schaeffler is the new Series and Innovation Partner of the German Touring Car Masters (DTM)
  • As preferred technology partner, Schaeffler is contributing to the electrification of the DTM with electric drive systems and steer-by-wire
  • Matthias Zink: “Collaboration demonstrates pioneering spirit and innovation, and underlines our desire, as technology partner, to make progress that has an impact on the world.”
  • New claim: “We pioneer motion”. As preferred technology partner, partnership underlines desire to make progress

At the final DTM race weekend of 2020, Schaeffler is showing what the future of the DTM will look like: it is green and electric. As the new Series and Innovation Partner of the DTM, Schaeffler and the umbrella organisation, ITR (Internationale Tourenwagen Rennen e.V.), are presenting a demonstration car at the Hockenheimring, which has four battery-powered Schaeffler drivetrains – one for each wheel – and is also equipped with Space Drive steer-by-wire technology. The prototype is driven by Formula E driver Daniel Abt and two-time DTM champion Timo Scheider, as well as Schaeffler Brand Ambassador, Sophia Flörsch.

“We are looking forward to the partnership,” said Matthias Zink, CEO Automotive Technologies at Schaeffler. “Our innovative e-drive technologies have been producing success in Formula E since 2014 and are now also used in production vehicles. The collaboration demonstrates pioneering spirit and innovation, and underlines our desire, as technology partner, to make progress that has an impact on the world.”

Demonstration car generates almost 1,200 hp
The demonstration car in action at the Hockenheimring generates almost 1,200 hp with 800 kW – that is virtually twice as much power as the current DTM cars (over 450 kW). The car accelerates from 0 to 100 km/h in 2.4 seconds, making it roughly 0.4 seconds faster than the current Schaeffler BMW M4 DTM. It also features Space Drive steer-by-wire technology, which has been successfully tried and tested in motorsport, as well as an integrated vehicle dynamics control to control the four motors. In its role as a development platform for the electric DTM, outings are planned at DTM events in 2021. It is then possible that the DTM will be a fully-electric race series from 2023.

“We pioneer motion”. Schaeffler loves partnerships, particularly when they nurture future technologies
The global automobile and industrial supplier has only recently launched a new image campaign, with the goal of positioning the corporate brand Schaeffler and communicating the new claim “We pioneer motion”. At the heart of the campaign is the concept “Green makes the difference”, which symbolises that Schaeffler is a trailblazer when it comes to motion. Matthias Zink: “The partnership with the DTM is perfectly suited to Schaeffler. As a pioneer, we want to challenge the status quo and push the boundaries – and, in doing so, to make a difference.”

You can find more information on the campaign at the microsite “We pioneer motion”.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept