Complete. Ready-to-install. Safe. FAG Complete Hub – the ready-to-install wheel bearing repair solution including hub for commercial vehicles from Schaeffler in the Automotive Aftermarket

2020-09-29 | Langen
- Easy installation for absolute safety and maximum service life
- Fast repair during initial installation and subsequent services
- Proven original equipment quality
With the FAG Complete Hub Schaeffler is extending its product portfolio for wheel bearing repair solutions of trucks and trailers and enables a simple and complete repair including the wheel hub. Depending on the application, the ready-to-install FAG Complete Hub unit contains the wheel hub including the respective Schaeffler wheel bearing repair solution FAG Repair Insert Unit, FAG Truck Hub Unit or FAG SmartSET, the ABS encoder ring and all accessory parts required for mounting, such as bolts and screws.
Highest safety and extended service intervals for maximum mobility
Wheel bearings are one of the most heavily stressed components in commercial vehicles. The repair is cumbersome and time-consuming. With the FAG Complete Hub, Schaeffler has developed a ready-to-install complete unit which is pre-assembled, pre-positioned and lubricated for life. This saves garages and fleet operators valuable time during the repair. Due to the reduced complexity of the repair, possible reasons for premature failure such as insufficient lubrication or ingress of dirt are eliminated right from the start. This allows garages to conduct a safe repair, minimize installation-related consequential damage and ensure a long service life of the components. What’s more: Thanks to the increased repair quality and the durability of the components, service intervals are extended and have a positive effect on the operating costs for fleet operators.
Fast and safe during maintenance or follow-up repairs
In the event of upcoming maintenance or, for example, brake repair, a mounted FAG Complete Hub allows for a fast repair because it always contains a pre-assembled wheel bearing unit from Schaeffler. Hub and wheel bearing always remain as a complete unit during disassembly and reassembly. There is no need to re-install the inner ring or re-lubricate the bearing which saves the garage additional time. This makes the FAG Complete Hub stand out from the competition – in particular in combination with the FAG SmartSET for vehicles with standard tapered roller bearings.
Proven original equipment quality
The FAG Complete Hub exclusively contains FAG wheel bearings in proven OE quality. Each product is subjected to strict quality control. A perfect bearing position and smooth, balanced running of the wheel bearing in the wheel hub are constantly tested. Of course, all components meet the quality standards of the series manufacturers. The range of 24 articles under the FAG brand comprises precisely fitting repair solutions for all common European applications.
Further information on FAG branded products and the complete Schaeffler product range for the automotive aftermarket can be found on the garage portal www.repxpert.com.
Publisher: Schaeffler Automotive Aftermarket GmbH & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)