Schaeffler steps up its involvement in Rear Wheel Steering

2020-09-21 | Herzogenaurach/Schwäbisch Gmünd
- New development partnership with Bosch Automotive Steering
- Intelligent mechatronic Rear Wheel Steering system delivers improved ride comfort and safety as well as superior energy efficiency
- Matthias Zink: “A key milestone in our journey to becoming the technology partner of choice for chassis systems”
Global automotive and industrial supplier Schaeffler is embarking on a development partnership with Robert Bosch Automotive Steering GmbH to expand its intelligent Rear Wheel Steering (iRWS) portfolio. The aim of the partnership is to grow the market by offering integrated solutions for Rear Wheel Steering systems. Under the partnership, Schaeffler is providing mechatronic iRWS systems, and Bosch Automotive Steering is contributing software and electronics in the form of steering control units. “Combining the strengths of both companies enables us to create integrated systems that deliver superior added value to our customers,” commented Matthias Zink, CEO Automotive OEM at Schaeffler. “Intelligent Rear Wheel Steering technology is a key milestone in Schaeffler’s journey to becoming the technology partner of choice for chassis systems.”
Rear-wheel steering technology: a mechatronic evolution
Schaeffler successfully launched its mechatronic intelligent Active Roll Control system (iARC) back in 2015. “The lessons we learned from that process flowed directly into the development of mechatronic Rear Wheel Steering”, said Dr. Keiwan Kashi, President Business Unit Mechatronic Systems at Schaeffler. “By combining our expertise in mechatronics with our core competencies in the industrialization of mechanical and mechatronic components, we created a highly efficient product that can be tailored to customer requirements.” The mechatronic iRWS unit improves ride comfort and safety which offers several key benefits in today’s rapidly urbanizing world. By turning the rear wheels in the opposite direction to the front wheels, it reduces the turning radius, significantly increasing maneuverability in tight spaces, such as when parking in busy urban settings. Moreover, the rear axle’s assistive steering action enhances handling, stability and ride comfort and improves vehicle safety. Schaeffler’s Rear-Wheel Steering system uses lightweight technologies and features a maximum overall weight of just eight kilograms. At the heart of the system is a planetary roller gear that performs a self-locking function, ensuring that the rear wheels do not change direction without steering input from the driver. The planetary screw drive also delivers superior efficiency. Moreover, the system’s design is acoustically optimized, making it particularly well suited for use in low-noise electric vehicles.
Bosch steering control unit supports safer driving
Bosch’s contribution to the partnership is the steering control unit, an integrated module comprising control electronics, an electric motor and software. Scalable and modular in design, this unit is fundamental to many of the driver-assistance functions in Schaeffler’s new rear-axle steering system. Already a proven performer, the steering control unit has been successfully implemented in millions of front-axle steered vehicles. It features Bosch security for robust protection against cyber attacks. Functions and updates are supported by over-the-air (OTA) technology. “Our third-generation steering control unit was launched just last year and is already doing very well in the market for front-axle steering control systems,” said Dr. Stefan Waschul, head of passenger car steering systems at Robert Bosch Automotive Steering. “Under this partnership, we will apply our expertise in this area to rear-axle steering systems and contribute the wealth of experience and technical know-how in software and E/E architecture that has made us the market leader in steering control systems.”
With decades of experience in software development and steering control, Bosch has already successfully partnered this technology in numerous customer applications. Based on signals from the steering wheel torque sensor, the steering control unit’s integrated electronic controller calculates the optimal steering assist, which is then delivered by the integrated electric motor. In addition to the torque applied to the steering wheel by the driver, the calculation takes into account numerous other vehicle parameters.
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)