Search term

Innovative components for robots and cobots Greater working radius: Schaeffler gives cobots greater range with plug-and-play linear actuators

Pressrelease Stage Image
Owners and users can significantly extend the working range of their cobots by installing Schaeffler driven linear units as horizontal axes.

2020-02-12 | Schweinfurt/Hannover

  • Plug-and-play linear actuators from Schaeffler add horizontal axes to extend the working range of robots and cobots
  • Ready-to-install turnkey system can be tailored precisely to customer requirements
  • Multi-part design enables linear travel distances of up to 18 meters

Industrial robots have long been established as the technology of choice when it comes to efficient automation solutions for a wide range of handling and processing tasks. Now, thanks to a new innovation, owners and users can significantly extend the working range of their robots and cobots (collaborative robots) by installing Schaeffler driven linear units as horizontal axes.

Plug-and-play linear axes made to order
Schaeffler offers its customers linear actuators as customized turnkey solutions. The compact, ready-to-install linear axis solution developed by Schaeffler consists of a MDKUVE tandem actuator, a corresponding adapter plate for the cobot, an appropriate motor/gearbox unit, prefabricated motor cables, a drag chain for all of the cobot’s supply lines/cables, and a motor controller. The solution comes complete with Profibus, Profinet, and EtherCAT interfaces for connection to the customer’s control system. The linear axis solutions have various options for connecting to the motor/gearbox units. Customers also have the option of using their drive technology instead of the Schaeffler drive solution if they so wish.

Depending on customer requirements, the linear axis can be supplied in various lengths and can be driven by a MDKUVE-KGT ball screw drive, a MDKUVE-3ZR toothed belt drive, or a linear motor.

In the tandem actuator, which forms the basis of the linear axis, the guide carriage runs along two parallel KUVE-type monorail guidance systems (four-row linear recirculating ball bearing and guideway assemblies). Because of its compact design envelope, the tandem actuator is ideally suited for use in applications involving high carrying and moment loads – such as collaborative robots. Tandem actuators offer maximum reliability in these applications when used in conjunction with triple toothed belt drives.

For applications requiring extremely high carrying and moment-load capacities, customers have the option of running the guide carriage on a KUSE-XL 6-row linear recirculating ball bearing and guideway assembly in X-life quality.

Increasing cobot range
The linear axes are available in a range of lengths, depending on the drive being used. They can even be implemented as multi-part axes for added range in applications involving longer travel paths. This flexibility means the compact linear axes be can easily integrated into new and existing automation solutions. As a further option, Schaeffler also offers an assembly and installation service.

Tandem actuators driven by ball screw drives are available in a range of lengths up to a maximum of 5.9 meters and offer repeat accuracy of 0.025 mm and a maximum linear speed of 1.7 m/s. Tandem actuators driven by toothed belt drives, on the other hand, can be implemented as multi-part axes with lengths of up to 18 meters for applications where especially long travel paths are required. These longer implementations support very high linear speeds of up to 5 m/s and offer a repeat accuracy of +/- 0.1 mm.

Because of their compact, high-performance design, these plug-and-play linear axes also have applications in areas other than collaborative robots, most notably in the periphery of handling and assembly equipment and in factory automation.

Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept