Schaeffler at the SPS 2019 (Hall 8 – Booth 311) Schaeffler will be exhibiting digital maintenance services at the SPS

2019-11-11 | Schweinfurt
- Schaeffler to appear at the SPS for the first time
- Digital services for rolling bearing applications
- Virtually hardware-free condition monitoring for auxiliary units
Schaeffler is set to make its first appearance at the SPS automation technology trade show – as a specialist for digital maintenance services. Schaeffler will be presenting both solutions for interpreting vibration and operating data from machines and facilities already equipped with sensor technology and for analyzing machines and facilities that are still entirely without sensors. Both of these market segments offer the processing industry significant potential for increasing OEE and open up growth opportunities for Schaeffler in terms of its own domain expertise.
In the majority of production facilities and machines, auxiliary units in particular have thus far been monitored either insufficiently or not at all. The consequence of this is that nobody has a complete overview of the machine’s condition that includes all of the subsystems and auxiliary units. At the SPS, Schaeffler will be demonstrating how this gap can be filled using its ConditionAnalyzer digital service, which automatically analyzes data from a range of wired vibration sensors and generates precise diagnoses. Schaeffler will additionally be presenting its ConditionAssistant application, which is a solution that requires virtually no hardware and analyzes further measurement data such as temperature and noise. Both of these applications give the customer digital access to Schaeffler’s domain expertise and generate tangible added value for maintenance technicians.
Rauli Hantikainen, head of the Industry 4.0 strategic business field, explains: “This gives operators and maintenance technicians a simple way of identifying specific rolling bearing failure mechanisms and interpreting the bearings’ condition, as well as putting relevant maintenance information at their disposal. Only when we have a complete overview of the condition of all our assets can optimized, reliable operation of machines and facilities be achieved without unplanned downtimes.”
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)