Search term

Sustainable Alternative Drive Systems Schaeffler develops and manufactures key components for fuel cells

Pressrelease Stage Image
Stacked bipolar plates form the core of the fuel cell system.

2019-10-15 | Herzogenaurach/Tokyo

  • Stacked bipolar plates form the core of the fuel cell
  • Materials technology, forming technology, and surface technology in perfection
  • Fuel cell makes important contribution to shaping sustainable mobility
  • Schaeffler presents its vision of innovation-led future mobility at the Tokyo Motor Show (South Hall 3/4, Booth S3203)

The irregular availability of renewable energies requires new energy carriers and electricity storage technologies. This is the only way to ensure sustainable mobility for tomorrow. Alternatives such as hydrogen, which is available in almost unlimited quantities on the earth, are becoming increasingly important here. Schaeffler has recognized the enormous potential of hydrogen technology as an energy carrier of the future and has developed key components for fuel cells and fuel cell stacks, so-called metallic bipolar plates. The company is using its traditional core expertise in materials technology, forming technology, and surface technology in this development work. Its main strength here is that it is strongly diversified in the industrial and automotive sectors and is thus involved at every point in the energy chain, from the generation of energy through to its use in vehicles. “We want to shape CO2-neutral, sustainable and individual mobility with regard to the entire energy chain”, says Uwe Wagner, Chief Technology Officer at Schaeffler. “The problem of global CO2 emissions cannot be solved with purely battery-driven vehicles alone. Heavy goods vehicles, in particular, will require alternative energy storage systems and hydrogen in combination with the fuel cell offers outstanding opportunities here. Hybrid storage systems, i.e. the combination of a battery and hydrogen, are also an attractive solution for achieving a longer range in passenger cars.”

The fuel cell is the key to sustainable mobility

Schaeffler has been focusing on the value added chain of key components for the fuel cell for some time and is using its traditional core expertise here. Bipolar plates are produced by precise forming and coating in the thin-layer range, which once stacked form the core of the fuel cell system. The fuel cell stacks are energy converters, which let H2 react with O2 to form water. The electricity generated during this process can be used to power the vehicle’s electric motor. Schaeffler’s portfolio for optimized fuel cell systems is expanded by additional areas of expertise, such as electronic control systems, special foil-air bearings, smart thermal management modules or components for passive hydrogen recirculation.

Schaeffler at the Tokyo Motor Show

Under the motto “Making Mobility Sustainable and Autonomous”, Schaeffler will be publicly presenting its holistic approaches for future, sustainable energy chains and CO2-neutral mobility solutions, including its expertise in fuel cells, at the 46th Tokyo Motor Show. The exhibits on the trade show booth will also include the new Schaeffler electric motors in various output classes that are now going into large-volume production and solutions for intelligent rear wheel steering. The range is rounded off by the Schaeffler Intelligent Corner Module with its 90-degree steering angle, drive-by-wire as a key enabling technology for self-driving cars, and the Schaeffler Mover as a new mobility concept for urban spaces. Visit us from October 24 to November 4, 2019, at the Tokyo Motor Show in South Hall 3/4 at Booth S3203.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept