From driver assistance systems through to comfort functions: One control unit does it all Getting connected for an autonomous future

2019-09-12 | Herzogenaurach/Frankfurt
- Schaeffler presents its innovative XTRONIC Control Unit as a basis for autonomous driving
- The Control Unit is not dependent on any specific platform, and it ensures a comprehensive range of safety, monitoring, operating, and comfort functions
- The solution is in volume production for several global OEMs
Remote monitoring and control are especially important for autonomous vehicles. However, such functions have thus far only been available in isolated systems or else have been dependent on specific platforms. The XTRONIC Control Unit on the other hand combines safety, monitoring, operating, and comfort functions in a single system. The innovative system also makes a convincing case thanks to its wide range of interlinked, integrated components – from entertainment systems through to condition monitoring for vehicle components. The reliable interlinking of innovative driver assistance systems together with radar, lidar, ultrasound, and even artificial intelligence thus provides the technological basis for autonomous driving.
Integration across platforms
The XTRONIC Control Unit allows digital control and monitoring to be combined in a single application for smartphones, tablet PCs, and smartwatches. The most important data are thus always available in the cloud and can be accessed from anywhere via mobile device. It doesn’t matter what type of vehicle platform is used for the implementation of the connectivity tools based on the control unit. Applications include not only (partly) autonomous vehicles but also commercial vehicles and motorhomes. The control unit recently went into volume production for several global OEMs to use in these fields of application.
CampConnect – the digital control system for campervans
At the IAA, Schaeffler will be demonstrating the advantages of this system using a campervan as an example. “CampConnect” is based on the XTRONIC Control Unit and allows comfort and safety functions in campervans and caravans to be digitally controlled. For example, end customers can access the full range of control functions and carry out status checks via smartphone while they are on the move. The owner can thus check the fuel level and the temperature, for example. Condition monitoring and predictive maintenance of components ensure availability and provide the basis for intelligent maintenance planning for both vehicles and entire vehicle fleets. If a break-in attempt occurs, an alarm is also immediately sounded.
About XTRONIC
XTRONIC has been part of Schaeffler since May 2019 and, as a technology partner, develops customized software and electronics solutions for the international automotive industry. The company’s service portfolio includes applications that range from automated driving and electric mobility through to functional safety as well as methods, tools, and testing systems – all of which makes XTRONIC a specialist when it comes to innovative interlinking for vehicles.
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)