Search term

Components and Systems for Increased Rigidity and Higher Loads Bearing solutions and dynamic motion systems for robot-based automation

Pressrelease Stage Image
INA XSU-series crossed roller bearings: Ideal for narrow design envelopes thanks to their high load carrying capacity and rigidity with a small bearing cross-section

2019-07-03 | Schweinfurt

  • Schaeffler offers the right bearing design for every robot joint
  • Optimized crossed roller bearings and double-row angular contact roller bearings for higher rigidity
  • Cost-effective, dynamic, and precise: Cartesian axis systems supplement portfolio for robotics

Industrial robots have established themselves in the competition for efficient automation solutions for a wide variety of handling and machining tasks. This development has been accelerated by increasing quantities and the associated fall in purchasing costs and by technical progress regarding rigidities and possible loads. Articulated arm bearing supports play a decisive role in the load carrying capacity, dynamics, and precision of robots. Schaeffler offers solutions for each of the six axes with their specific requirements.

Swivel joint bearing supports for articulated robots
The lower swivel bearing support for axes 1 and 2 of a robot supports the entire weight and the largest tilting moments. What makes things even more difficult is the fact that tilting in the bearing support is multiplied as far as the tool center point (TCP). This is where Schaeffler offers INA ZKLDF double-row axial angular contact ball bearings with very high tilting rigidity, which are well known from the machine tool sector. Their solid bearing rings are screw mounted to the adjacent construction.
Axes 3 and 4 still support a significant proportion of the robot arm’s weight, however, the installation space in the joint is already significantly restricted. This calls for a high load carrying capacity and rigidity with a small bearing cross-section. Schaeffler’s engineers have optimized INA XSU-series crossed roller bearings especially for the increasing requirements in this application. A particularly high filling level with cylindrical rollers ensures increased rigidity.
Double-row bearing supports, particularly those in an O arrangement, offer major potential for bearing supports with very high tilting rigidity due to their very large support distance and small axial design envelope. INA SGL-series angular contact roller bearings also have a very rigid roller contact. Schaeffler recommends a combination of both types, particularly for axes 5 and 6 with small articulated arm diameters. SGL bearings can be very flexibly integrated into the available installation space between the robot’s gearbox and the housing due to their small cross-section and diameter graduations.

The 7th axis – the extended arm
A so-called 7th axis is frequently used to extend the working area of industrial robots or enable them to move greater distances. The robot is moved between individual machine tools or stations and the magazines and palette systems on a table of the linear axis. The INA KUSE six-row monorail guidance system in X-life quality is particularly suitable as a guidance system here. It offers a very high nominal rating life, reduced lubricant requirement, and extremely small stroke pulsation. In a compressive direction, this six-row monorail guidance system has a particularly high load carrying capacity and is therefore ideally suited for combination with direct drives. In order to maximize the availability of the entire production cell with X machine tools, Schaeffler offers DuraSense as an option for its monorail guidance systems. DuraSense’s integrated sensor system enables automated lubrication or monitoring of the lubrication condition of carriages. The risk of unplanned downtimes due to wear and lubrication failure is significantly reduced.

Cartesian systems: Cost-effective, dynamic, and precise
It is not always necessary to use an expensive robot for handling workpieces and tools. These tasks can be frequently still performed by cartesian axis systems, which are constructed from linear actuators that can be combined. Schaeffler offers an extensive range of INA linear actuators and driven linear units in this field. Linear actuators with special functions expand the range of applications. MTKUSE telescopic actuators, for example, allow a handover in areas behind protective barriers or in separate workspaces.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept