Sensor System for Reliable Operation of Linear Guidance Systems Schaeffler DuraSense increases the effectiveness of the overall system

2019-07-03 | Homburg
- Automated, requirements-based relubrication of INA monorail guidance systems with monitoring of the entire lubrication system
- Option for monitoring manual relubrication systems
- Changeover to lifetime lubrication without risk
- Indirect monitoring of extreme operating conditions and events
Schaeffler DuraSense is designed for the safe operation of INA linear recirculating ball or roller bearing and guideway assemblies and monitors the tribological conditions of linear guidance systems based on vibration signals. The system comprises carriages with sensors developed specifically for this task and a pre-processing unit for up to seven sensors. The pre-processing unit is at the heart of DuraSense and contains Schaeffler’s rolling bearing expertise, evaluates the sensor signals, and generates an authoritative parameter, the lubrication parameter. The vibration energy that is emitted by the carriage is affected as the lubricant ages or the quantity of lubricant becomes less, and the Schaeffler DuraSense makes use of this effect. The lubrication parameter measured during measurement runs describes the carriage’s current lubrication condition and Dura Sense sends a signal to the machine’s control system if a lubrication limit value generated based on the bearing’s new condition (i.e. the target situation) is exceeded. As an option, Schaeffler DuraSense can be combined with a lubrication system from Schaeffler (Concept2 or Concept8). Schaeffler DuraSense provides various options for increasing the effectiveness of the overall system depending on the application.
Schaeffler DuraSense can detect both correct relubrication and insufficient relubrication. An unforeseeable and premature machine downtime caused by insufficient lubrication or a failure to perform relubrication and maintenance – a nuisance for the machine manufacturer and operator – is therefore a thing of the past.
Initial operation of Schaeffler DuraSense
A service setup tool is used for configuration and initial operation. For this purpose, the pre-processing unit is connected to a PC via an ethernet interface. The lubrication condition and the lubrication limit value are measured and displayed during a subsequent reference run with a freshly lubricated carriage. The log files for the measurements can be read out and updates loaded via the ethernet interface if required.
Lubrication condition as an analog or digital signal
The pre-processing unit can transmit digital signals 0 – 24V or analog signals 4 20 mA to the machine’s control system. The digital signal indicates whether the lubrication condition of the carriage corresponds to the target situation or whether relubrication is required. The analog signal enables a differentiated analysis of the lubrication condition and provides the option of using the lubrication parameter for further more detailed analyses.
Increased effectiveness of the overall system
Schaeffler DuraSense makes the lubrication condition of the carriage transparent and indicates critical lubrication levels. This enables a conversion to manual lubrication in linear axes, which e.g. are only connected to a central lubrication system for safety reasons due to low loads and short periods of operation. The machine layout is thereby simplified and the costs for the pipework connection to the central lubrication system including the metering valve can be saved. Overgreasing or an accumulation of grease and the risk of contaminated workpieces – a common phenomenon when central lubrication systems are used – can also be prevented.
Since Schaeffler DuraSense monitors the changes in the lubrication condition on the carriage, the system detects all the defects and changes that can affect lubrication. This includes all defects in the lubrication system and defective guidance system covers and the influence of cooling lubricants etc. Schaeffler DuraSense notifies the control system that relubrication is required before the next, defined lubrication interval. This enables a troubleshooting function in the event of unusually short relubrication intervals. In highly automated manufacturing systems with considerable interlinking of machines, entire production lines can be protected against unplanned downtimes in this way, which significantly increases the effectiveness of the overall system.
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)