Search term

Innovative Monitoring System for Spindle Bearings Schaeffler SpindleSense reduces machine downtimes and increases utilization of machine capacity

Pressrelease Stage Image
Design of the Schaeffler SpindleSense monitoring system: 1 Distance sensors; 2 Evaluation unit; 3 Connection cable

2019-07-03 | Schweinfurt

  • Electronic protection against continuous overload and collision damage
  • Sensor ring monitors displacement of the spindle bearing with micrometer precision
  • Measurement of displacements in combination with Schaeffler’s expertise in rolling bearings enables assessment of operating conditions
  • Detection of critical operating conditions within 2 milliseconds

The main spindle is crucial to the performance capability of the complete machine tool. It is at the heart of the machine and largely defines the achievable cutting capacity, surface quality, and precision. In turn, the spindle bearing support is one of the most heavily loaded components because it must transmit machining forces precisely at very high speeds for long periods of time and the risk of collisions can never be ruled out. It therefore comes as no surprise that the majority of machine tool downtimes can be traced back to defective spindles, particularly as a result of collisions and continuous, undetected overloads. In milling operation, for example, the combination of high radial loads, long tool protrusions, and high speeds leads to particularly high loads and unfavorable kinematic conditions on the spindle bearing in the vicinity of the tool. These unfavorable and in some cases impermissible loads occur because operators have hitherto not had a suitable tool, with which they could monitor borderline loads on spindle bearings. Schaeffler has now solved this problem with its new SpindleSense monitoring system.

Ready for volume production to coincide with EMO 2019

The first production-ready SRS sensor ring units including radial and axial measuring ring with an inside diameter of 70 mm will be available for customers to test in practical applications to coincide with EMO 2019. Additional sizes with 80 and 100 mm inside diameter will be available at the end of the year. All units have a standard width of 16 mm. The scope of delivery includes an SST setup service tool, with which SpindleSense can be parameterized and put into operation.

The sensor system integrated into the spindle bearing measures the displacement of the spindle shaft under load in a very high resolution and in five spatial directions – three translational and two rotatory. The sensor ring transmits an electrical warning signal to the machine’s control system if the deflections measured on the rolling elements exceed a specific threshold, which is set individually for every spindle and machine type. The threshold is based on an assessment of operation-related bearing parameters such as pressure, spin/roll ratio, and cage pocket clearance, into which Schaeffler has integrated its many years of expertise in rolling bearings.

Software with rolling bearing expertise integrated into sensor ring

All of the software and the required algorithms are integrated into the 16 mm wide sensor ring. No further components are required for the system. The system is locally functional and transmits an individual warning signal to the machine’s control system, which makes the following applications possible:

  • Detecting a crash (collision): The sensor technology is capable of signaling an overload at a digital output within 2 milliseconds. This allows serious subsequent damage to be minimized or even prevented through fast deactivation of the drive.
  • Long-term protection for machine tool spindles: In practice, continuous mechanical spindle bearing overloads are not immediately identified. In contrast, SpindleSense immediately triggers a warning signal when the overload is parameterized accordingly. The operator can adjust his machining program right after the first manufactured part and reduce the spindle load by using a new tool or modified cutting values, or by employing a more suitable tool type. The operator thus achieves lower and less numerous peak loads, and thus benefits from a longer spindle operating life with fewer machine tool downtimes, which ultimately means more production time and reduced repair costs.

Two options are available for outputting the measured values. Variant C-A0 transmits alarm signals as soon as the individually defined limit values for the bearing load and kinematics are reached. Variant C-A1 outputs the measured radial and axial displacements including tilting via CAN bus. Machine tool and spindle manufacturers can use these displacement values to develop analysis tools for optimizing the utilization of spindle capacity, e.g. by visualizing the deflection collective measured by the sensor ring as a load collective. For the first time ever, the machine operator will know the degree to which the spindle capacity in each machining process is being utilized as a percentage with a high level of accuracy and thus be able to adjust the machining process even more precisely in terms of capacity utilization and operating life for each machine: This means that harmful overloads are prevented despite maximum spindle loads. Safe operation in the limit range allows the operator to increase his or her productivity and also to benefit from longer spindle operating life and less frequent machine downtimes.

The measured displacements that are outputted via CAN bus can also be used for zero point compensation. This makes it possible to produce the same quality with larger cutting values or higher quality with unmodified cutting values. The monitoring of the maximum displacement can also be used for quality assurance.

Electronic versus mechanical overload system

In comparison with mechanical, i.e. passive overload systems, Schaeffler SpindleSense does not just protect the spindle in the event of a collision, it is also a revolutionary system for safely maximizing the utilization of the spindle capacity. For the first time ever, machine manufacturers can now offer their customers a highly effective tool for increasing productivity, machine availability, and quality.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept