Schaeffler at the Hannover Messe 2019 (Hall 22, Booth D43) Schaeffler combines condition and torque monitoring in one single system

2019-03-22 | Schweinfurt
- Industry 4.0 pilot project for the wind power industry presented in Hannover
- Innovative TorqueTracking system for industrial drives
- Vibration analysis and torque monitoring combined in a single system
- Customers benefit from increased drive availability and longer maintenance intervals
The long-term development partnership of Schaeffler and Bonfiglioli, market leader in yaw and pitch drives for wind turbines, lead to the creation of a compact Industry 4.0 solution package. Schaeffler has combined two of its proven measuring systems, the SmartCheck and the TorqueSense to create a new condition and torque monitoring system. While the vibration diagnosis system of the Schaeffler SmartCheck detects incipient damage at a very early stage, peak loads as well as their frequency can also be detected and limited using the precise torque signal. Using algorithms that are based on their application expertise, Bonfiglioli converts such data into information throughout the entire lifetime of a wind turbine. Thus, online reporting on relevant performance indicators is provided, e. g. the general “health” status of the geared drives, possible critical conditions, and abnormal behavior of the yaw systems. In total, customers benefit from reduced unplanned downtimes as a result of overloading or unexpected operational conditions of the system and load-based (i.e. generally longer) maintenance intervals due to predictive monitoring.
A clever combination
The Schaeffler SmartCheck device performs frequency-selective condition monitoring of bearings, gearboxes, electric motors, pumps, fans, and machines based on solid-borne vibrations. Conspicuous frequencies can be automatically attributed to the damaged component using only one Schaeffler SmartCheck. A temperature sensor is also integrated into the device. The torque signal and speed signal of the Schaeffler TorqueSense are sent, preprocessed and supplied to the machine control system and/or maintenance department with the vibration signals that are also analyzed via the SmartCheck. The addition of operating data on torque and speed to the SmartCheck condition monitoring system opens up several new scenarios. In the simplest case, the system allows the monitoring of torque peaks and their frequency and thus an evaluation of the utilization level and the derivation of load-based maintenance measures. The signals can also be integrated into the operating strategy for drives and initiate torque limitation or shutdown functions. The new system is particularly suitable for adjustment and rotary drives in the wind power and shipbuilding industry, in large cranes, construction and mining machinery with turrets, and for winches. The torque signal can be used for both monitoring and smooth and precise torque control and regulation of the pull cable.
Pilot project for the wind power industry
Schaeffler is currently developing an initial pilot project for Bonfiglioli’s geared motors of yaw drives for wind turbines. In this application, the load data that are condensed using the Schaeffler SmartCheck are compared with predefined limit values and the results are transmitted wirelessly to Bonfiglioli via a gateway. The monitoring system for Bonfiglioli geared motors operates independently and is not connected with the turbine’s control system, making it very easy to retrofit when the geared motors are replaced. With the new system, Bonfiglioli aims to monitor overloading of the yaw drives, increase the lead times for maintenance, and make it possible to define load-based instead of time-dependent maintenance procedures. The TorqueSense module is positioned between the motor and gearbox to integrate it into the flow of force of the geared motor. The measurement system is also fully functional in lubricating oil and offers significant advantages for integration into the drive train such as:
- high measurement accuracy (approximately 1% of the measuring range) at an attractive price,
- non-contact measurement principle,
- no change in the load carrying capacity and torsional rigidity due to the sensor shaft,
- temperature has a minimal influence on the operating life and measurement accuracy, and
- integrated speed measurement.
Torque sensor technology can be easily integrated
Schaeffler TorqueSense comprises a magnetically conditioned section of shaft and a sensor housing. The housing does not have to completely surround the shaft. Designs that are mounted on one side only or U-shaped designs are possible depending on the required accuracy and interference immunity. Because a non-contact measurement principle is used, the torque can also be measured from outside by means of a non-magnetic housing. The sensor module can then be mounted from the outside. With Schaeffler TorqueSense, customer and application-specific shaft diameters of up to approximately 100 mm are possible; sensor units in different standard diameters already exist. The measuring range is from 100 Nm to 20 kNm. The sensors have high linearity and extremely small hysteresis due to the measurement principle used.
Further press releases regarding the innovations that Schaeffler will be presenting at the Hannover Messe can be found in our press kit: www.schaeffler.com/press-kit/hannover-messe
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)