Schaeffler at the Hannover Messe 2019 (Hall 22, Booth D43) Finished in a matter of seconds: Insert, drive in, and the job is done.

2019-03-08 | Homburg
- Outstandingly fast and secure mounting of Schaeffler’s profiled guide rails thanks to new patented closing plugs
- Innovative design of closing plugs shortens the mounting time more than fourfold in comparison to other systems
- Wall and overhead mounting of profiled guide rails is made significantly easier
Closing plugs for profiled guide rails have to perform significantly more functions than may at first be apparent. The top priority for many customers is fast and simple mounting, a minimal annular gap between the plug and guide rail surfaces, and a high retaining force. Schaeffler fulfills these essential customer requirements with its new patented KA-TN/B closing plugs. The KA-TN/B plastic closing plugs have a special feature: The plastic plug is joined to the respective component by means of a clinch ring. Mounting the closing plug simply involves inserting it into the bore and then driving it in until it is flush with the surface. There is a predetermined breaking point between the clinch ring and the plug, which comes loose when the plug is driven in, while small clamping lugs on the clinch ring hold the closing plug securely in position in the bore. This innovative design now makes it possible to manually place several closing plugs into the bores and drive them in one by one in a single working step. This shortens the mounting time more than fourfold in comparison to other systems. The previously very complex tasks of wall and overhead mounting thus no longer pose any problems. Any tilting of the closing plug while it is being driven in is virtually eliminated by the clinch ring’s guidance. The small dimensions of the annular gap between the closing plug and the counterbore make it virtually impossible for fluids and contamination to accumulate there, and ensure that the guide carriage is well-sealed.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Press releases
Package (Press release + media)