Schaeffler at the Hannover Messe 2019 (Hall 22, Booth D43) New cover strip for profiled guide rails from Schaeffler reduces mounting times by up to 90 percent

2019-03-08 | Homburg
- Reusable slide-in cover strip shortens cycle times when mounting multi-axis systems
- The axis’s fixing screws remain accessible and can be perfectly adjusted as often as necessary with the carriage still mounted
- The entire length of the guide rail can be used thanks to a countersunk screw joint at the end of the guide rail
With their innovative new cover strip for profiled guide rails, Schaeffler’s linear technology specialists will be presenting a very simple and practical mounting solution: The ADE steel cover strip is slid into a fitted groove in the guide rail and fixed in place using a screw. Mounting times are thus reduced by up to 90 percent in comparison with previous solutions. This means that, in the mechanical engineering sector, cycle times in the assembly of multi-axis systems can be drastically reduced. The new cover strip is currently available for RUE 35, 45, and 55 linear recirculating roller bearing and guideway assemblies, with further variants set to follow. It is also reusable and offers decisive advantages in both initial operation and maintenance: Unlike other solutions, the ADE cover strip does not have to be mounted in the profiled guide rail during the machine construction process. This can also be done subsequently. All of the axis’s fixing screws remain accessible and can be perfectly adjusted as often as necessary with the carriage still mounted. The carriages’ seal lips do not touch the counterbores in the profiled guide rail and damage to the seal is eliminated. Once the guide rails have been mounted and the geometry check has been completed, the cover strips are simply inserted into the profiled guide rails and under the seal lips of the guide carriages. It is fixed into place in the groove using a countersunk screw joint at the end of the guide rail. This means that the entire length of the guide rail can be used.
In the case of single-piece guide rails, the customized cover strip is delivered in the packaging together with the guide rail and carriage; for multi-piece guide rails, the cover strip is rolled into a coil and packaged together with the carriages and guide rail sections.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)