Schaeffler at the Hannover Messe 2019 (Hall 22, Booth D43) Digital twins via REXS: Schaeffler digitalizes the development process in gearbox construction

2019-03-08 | Schweinfurt
- Gearbox development with REXS: Standardized and fully digitalized data transfer replaces manual data transfer
- Schaeffler customers not only benefit from significantly shorter development times
- The new REXS data interface provides the basis for simplified digital twin generation
A complete virtual representation of drive trains and gearboxes is only possible when gearbox, rolling bearing, and gearing specialists can digitally link their simulation models together. This makes the exchange of data across companies and systems one of the most important prerequisites for the generation of digital twins. A number of specialized software and CAE tools for designing and simulating gearboxes have established themselves on the market, each of which has its own specific points of focus. The problem, however, is that manufacturers and their suppliers still often exchange gearbox data manually, which causes time-consuming duplicate work. In collaboration with SEW-EURODRIVE and the FVA (Research Association for Power Transmission Engineering), Schaeffler has now developed an electronic data transmission system that replaces this manual exchange between CAE tools and eliminates repeated gearbox modeling processes by means of a standardized interface for gearbox data. Development times are thus significantly shortened and a basis created for the generation of digital twins that can be used to analyze operating data as part of Industry 4.0 solutions, for example.
Standardized data format in gearbox construction
The format is known as REXS (Reusable Engineering Exchange Standard), and version 1.1 offers a standardized modeling system and nomenclature for any desired gearbox with spur gear, bevel gear, and planetary gear stages as well as their components. REXS is currently integrated into the FVA Workbench from version 5.0 upwards, into all current versions of Schaeffler’s Bearinx rolling bearing analysis tool, and into SEW-EURODRIVE’s WESILAB gearbox calculation program. Even commercial CAE tool suppliers have now implemented the REXS interface or are planning its introduction as part of their next releases. A simple mouse click is all it takes to generate an REXS file from the gearbox models.
Schaeffler now offers the automatic exchange of gearbox data via the REXS interface. Customers obtain calculation results from Bearinx significantly faster, which considerably speeds up their development processes. Stephan Evert, Head of Bearing Analysis Tools Development in Schaeffler’s R&D Bearings department, spoke emphatically about the advantages: “REXS allows us to reduce the outlay for linking CAE tools and simulations in the relevant software systems while simplifying the IT architectures at the same time.” He went on to explain: “REXS can be used by the gearbox sector as a standardized data container for the generation of digital twins.”
Faster application development in gearbox construction
Gearbox manufacturers with a high proportion of customer-specific application development benefit greatly from being able to digitally exchange data with their suppliers. “The objective is to allow different systems that have their own focal points in terms of calculation to be used efficiently and effectively”, explained Dr. Heinrich Bolz, Head of Calculation and Simulation in Gear Unit Development for SEW-EURODRIVE. Regarding the open-source project, he continued: “With REXS, gearbox data can be transferred quickly and without errors, which means the interface makes an essential contribution to the optimization of our innovation process.”
The REXS interface is freeware, and is available at www.rexs.info together with all further information about current and future developments.
Visitors to Schaeffler’s trade show booth can watch a live demonstration that shows just how easy it is to exchange data models between CAE tools.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)